SupplyHouse Blog Banner 2





Fasco Motors

Adam

Fasco Motors have arrived at SupplyHouse.com just in time for the heating season! Fasco Motors manufactures top of the line OEM replacement Motors and Draft inducers for the biggest names in the HVAC industry. Here you can find replacements motors and draft inducers for Lennox, ICP/Heil Quaker, Trane, York, Goodman, and many more.

A draft inducer is a fan that operates when there is a call for heat. It blows air into the vent at the beginning of the heating cycle to ensure the vent to the outside is clear. If the vent is not clear, combustion gases will get inside the home and cause problems. The draft inducer starts operating before the flame is lit and continues running while the flame is burning. If the draft inducer is supposed to be running and the furnace realizes it is not, the furnace will shut off. A furnace will not run without the draft inducer, which means you will not have heat. Don’t get stuck without heat this winter. Fasco Motors are in stock and ready ship today!

Posted in All Posts, Products | Tagged

Comments are closed.


Logo

Join Our Mailing List - Sign up and receive special offers and coupons