SupplyHouse Blog Banner 2





Art Cool Mini-Splits For Comfort—And Décor

Kristine

Making a room cool doesn’t have to involve loosing a window. Today’s mini-split air conditioning units are the smart alternative to traditional window units, delivering comfort and decor all in one.ArtCool-LG-LAN096HNP_2-crop

Summer has arrived, and with the inexorable heat comes the inevitable hunt—for the perfect air conditioner, that is. Homeowners in search of a functional and fashionable alternative to conventional air conditioning units may want to consider a mini-split.  Mini-split air conditioning systems eliminate the need for the extensive wiring and ductwork required for central air systems, making them perfect cooling devices for older homes and new additions.  They also alleviate many of the problems associated with standard window units, namely they are quieter, don’t have to be removed “off-season,” and don’t present a bulky and unattractive appearance in the window. And, if it’s appearance that you are concerned with, LG’s Art Cool Mini Splits were made for you.

ArtCool-LG-LAN096HNP_11“The Art Cool series is a unique take on the tried-and-true mini split air conditioning formula,” explains Daniel O’Brian, a tech team member here at SupplyHouse.com. “While being functionally the same (and in the same price range as standard mini split systems), they offer a more visually pleasing indoor unit that can actually enhance room decor,” he adds.

LG’s Art Cool line basically consists of two options, both of which come in either air-conditioner-only or heat-pump models: Art Cool Mirror units feature a flat panel surface with smoked charcoal mirror finish, creating a sleek, contemporary silhouette; and the Art Cool Gallery unit provides a 20-by-20 inch square panel that works like a picture frame—allowing the consumer to insert their own artwork or photograph. Both units mount securely on a vertical surface with screws.

Mini-split air conditioning systems typically consist of two separate units: an interior evaporator with a fan and cooling coil, and an outside condenser unit; the two pieces are connected by a refrigerant line set. Mini-split systems are available in single room configurations, which consist of one indoor unit and one outdoor condenser, as well as multi-room configurations, which have two to four indoor units connected to a single outdoor condenser. Most mini-split indoor units are mounted on the wall, although there are some ceiling-mounted versions.artCool-LG-Mirrorfinish-b

The LG Art Cool Gallery unit is available as a single zone system in either 9,000- or 12,000-BTU sizes; the Mirror units are available in either single- or multi-zone systems. Choosing the appropriately sized unit is dependent on several factors, including the regional climate, whether the mini split system will operate as a cooling unit only, or a combination of cooling and heating, the number and type of rooms, the number of windows per room and the average number of people occupying the room at a single time. SupplyHouse.com features a useful air conditioner sizing calculator to help consumers determine the correct amount of air conditioner BTUs needed for a given room, or set of rooms.

Typically, mini-split air conditioners will require professional installation by an HVAC (heating, ventilation and air conditioning) contractor, because the outdoor unit must be hard-wired to a dedicated circuit breaker and the correct amount of refrigerant must be used in the lines.

SupplyHouse.com offers a large selection of mini split air conditioners and accessories from the top manufacturers in the industry.  To learn more about the LG Art Cool systems, view the video below, or visit SupplyHouse.com.


This post was written in collaboration with Bob Vila

Posted in All Posts, Products | Tagged

Leave a Reply

Your email address will not be published.


Logo

Join Our Mailing List - Sign up and receive special offers and coupons