SupplyHouse Blog Banner 2





Search Results for: pex


Bluefin PEX Fittings

Emily

  These lead-free barbed fittings work for PEX connections and may be used with the copper crimp ring system or the stainless steel clamp system.   Bluefin PEX fittings come in poly and brass material.  They come in different styles … Continue reading

Posted in All Posts, Products | Tagged , , , , , , , , , , , , ,

PEX Press w/ Milwaukee

Mark

The Milwaukee M18 Short Throw Press Tool is the fastest way to make PEX Press connections on the market today.  40% faster than the competition, this tool will get your job done fast.  Watch the video below to learn more!     … Continue reading

Posted in All Posts, How Tos + Tricks, Products | Tagged

How To: Connect PEX to Copper or PVC

Guest

Today, with the help of cross-linked polyethylene (PEX) pipe, plumbing work has become more efficient for professionals and much more accessible for do-it-yourselfers.  These flexible red and blue pipes can bend in nearly any direction to funnel hot and cold … Continue reading

Posted in All Posts, How Tos + Tricks, Products | Tagged , , , , , , , , ,

Will It Bend? PEX Tubing

Nick B

The answer is yes, obviously.  That’s one of it’s main selling points.  It even comes in rolls.  But the real question is will PEX-A bend better than its competition?  Can PEX-A withstand more abuse?  Well we set out to discover … Continue reading

Posted in All Posts, Products | Tagged , , , , , , , ,

Tools for PEX Connections (Crimp, Clamp, Expansion, Press)

Guest

PEX revolutionized plumbing in more ways than one, including making it easier for pros and DIYers alike.  Still, if you’re new to PEX tubing, there’s one tricky aspect to navigate at the outset—that is, choosing a method of connecting one … Continue reading

Posted in All Posts, How Tos + Tricks, Products | Tagged , , ,

The Types of PEX (PEX-A, PEX-B, PEX-C, PEX-Al-PEX)

Guest

For much of the latter 20th century, household plumbing systems depended on copper pipe—a difficult-to-master building material whose price only rose along with the ever-increasing demand.  Today, many pros (and do-it-yourselfers) prefer to use tubing made of cross-linked polyethylene, or … Continue reading

Posted in All Posts, Products | Tagged , , , , , , ,

PEX-AL-PEX: Tubing with a Little Backbone

Tom

PEX pipe works in a wide variety of heating and plumbing applications, offering major benefits including cost savings.  In the decades following the introduction of PEX, manufacturers developed a variation of PEX that includes a layer of aluminum.  PEX-Aluminum-PEX, generally … Continue reading

Posted in All Posts, Products | Tagged , , , ,

Facebook Live Seminar: Uponor’s PEX Tubing

Mark

For the second installment in our Facebook Live series we brought in a couple experts on Uponor and their PEX tubing. (Watch the first one on Taco here)  Wes Sisco from Uponor fielded questions from our audience using his years of … Continue reading

Posted in All Posts, How Tos + Tricks, Products | Tagged , , , , ,

PEX: Uponor’s Contribution to the World of Plumbing

Nick B

The modern day Uponor is the culmination of two longstanding and innovative companies.  Uponor’s origins date back to a Finnish carpentry workshop opened in 1918 while the other half, Wirsbo, began in the 1620s as a Swedish forge, crafting top … Continue reading

Posted in All Posts, Products | Tagged , , ,

How to Make ProPEX Expansion Connection

Mark

Uponor’s ProPEX expansion connection system is a reliable and easy connection method for PEX-A tubing that actually becomes stronger over time. Using an expansion tool that features an auto-rotating head, like the Milwaukee M12 Tool, connections can be made in under … Continue reading

Posted in All Posts, How Tos + Tricks, Products | Tagged , , , ,

Is PEX Here to Stay?

Nick B

  Earlier today I decided to look up our first ever blog post.  No, it’s not Welcome to the SupplyHouse.com Blog, this post was on our old blog, before most of the people here worked with us (myself included), numerous website … Continue reading

Posted in All Posts | Tagged , ,

Making Connections: PVC to PEX

Nick B

Looking to connect a PVC pipe to PEX?  Well there are a couple options available to tackle this project.  They range from the tried and true threaded adapters to the fast and easy SharkBite fittings.  Threaded adapters have been plumbers’ choice … Continue reading

Posted in All Posts, How Tos + Tricks, Products | Tagged , , , , , , , , ,

SupplyHouse.com Logo

Join Our Mailing List - Sign up and receive special offers and coupons