Home 2014 March

Monthly Archives: March 2014


Takagi T-H3 Tankless Water Heaters

Tom

Tankless water heaters offer the potential for increased efficiency because they do not waste energy heating water during periods of non-use. Takagi’s T-H3 Series of gas-fired tankless heaters offers several useful features in addition to extra efficiency. Created as new-generation … Continue reading

Posted in All Posts |

Motors & Armatures, Inc, (MARS)

Adam

Motors & Armatures, Inc, (MARS) was founded in 1946, and is known for being one of the biggest providers of replacement parts in the HVAC/R industry. MARS is a family-owned and operated supplier of quality motors, components and service and … Continue reading

Posted in All Posts |

Floor Sensors for Radiant Heat

Tom

Using a floor sensor is usually considered the most precise way to control an in-floor hydronic heating system. Surface temperatures above about 87°F can make floors uncomfortably hot to walk on. Wood flooring in particular can be damaged by excessively … Continue reading

Posted in All Posts |

Welcome to the SupplyHouse.com Blog

Kristine

We’re in the process of changing our name from PexSupply.com to Supplyhouse.com! We are still the same people committed to providing the same great service we always have, under a name that better represents the broad range of products we … Continue reading

Posted in All Posts |

Lead-Free Plumbing Law

Tom

The Reduction of Lead in Drinking Water Act in the United States went into effect earlier this year, on January 4. The act imposes standards that were already enforced in several states. It defines “lead-free” as less than .25% lead … Continue reading

Posted in All Posts, Plumbing Supplies |

GV90+ Boilers from Weil-McLain

Tom

Weil-McLain’s GV90+ series of gas boilers presents a unique option for hydronic heating systems: cast iron condensing boilers. Condensing boilers can handle condensed flue gases when return water temperatures are sufficiently low, resulting in less waste and higher efficiency ratings. … Continue reading

Posted in All Posts, Boilers, Heating Supplies |

Grundfos UP Zone Valves

Adam

The Grundfos range of UP Zone Valves (UP-ZV) are designed to control your comfort with the latest in robust motor and gearing technology, to ensure long life and quiet operation. The UP-ZV range is designed for closed water heating and … Continue reading

Posted in All Posts, Boilers, Heating Supplies |

Logo

Join Our Mailing List - Sign up and receive special offers and coupons