Boiler Room |
Radiators & TrimGas Products |
Specialties |
Your new password is on its way. If you have problems accessing your account, please contact us at 1-888-757-4774 and we'll help you out.
I'm sorry, your e-mail was not found in our system.
If you think this is a mistake, please contact customer service at 1-888-757-4774 or via e-mail here.
You will have the option to create an account on the order confirmation page.
New from Honeywell, the Ultraviolet Air Purifier with AirBRIGHT Odor Absorption uses ultraviolet light to help keep your air clean. The system can eliminate up to 99 percent of mold spores on the air conditioning coil, which will help to … Continue reading →
Hey, here’s episode 9 of “PexTV” but its also kind of like episode 467…This weeks episode gets a visit from a special guest. You won’t want to miss who it is… In this episode, you’ll see… Featured Product: Honeywell RedLINK … Continue reading →
Polybutylene (PB) piping was commonly used for domestic water piping in the United States during parts of the 1970s and 1980s. Polybutylene can be identified by its gray color. Lawsuits related to fitting assembly failures caused the production of PB … Continue reading →
New to SupplyHouse.com, John Guest’s PEI Twist & Lock UV resistant Push-Fit Black Fittings come in 3/4” and 1” CTS sizes. The fittings are manufactured from high quality engineered plastic with EPDM ‘O’ rings ensuring a leak-free and lead-free connection. … Continue reading →
J-B Weld Company of Sulfur Springs, TX (903-885-7696) told me that the City of Dallas, Texas used their product to repair a cracked Caterpillar engine block. That sure got my attention! They also said that people have been using J-8 … Continue reading →
Released earlier this year in the United States, the Multi F Max ductless mini-split condenser from LG makes large mini-split systems possible without multiple outdoor units. The Multi F Max carries a 54,000-BTU rating, and can serve as an air … Continue reading →
It’s important to remember that when buying fittings for plumbing and heating systems, copper pipe sizing refers to the listed size of the pipe which is approximately the inner diameter. For example, a ½ inch Copper fitting doesn’t actually measure … Continue reading →
Air King’s reversible Window Fans are available in sizes to fit virtually any window. These whole house window fans can save the average homeowner a small fortune compared with an air conditioner, and are great to use as an alternative … Continue reading →
Hey, here’s episode 7 of “PexTV” It’s fan appreciation day here at PexTV and we are going to tell you about Fantech!. Feel free to email us at pextv@supplyhouse.com with any thoughts or suggestions for future episodes. In this episode, … Continue reading →
Does it seem like it takes forever for your clothes to dry? The solution may be easier than you think. With a Fantech Dryer Booster Exhaust Fan from SupplyHouse.com you can cut down on clothes drying times and slash your … Continue reading →
The Gas Ox Box from Sioux Chief is a Gas Outlet Box used for applications involving a connection to a gas line, such as Furnaces, Water Heaters and Gas Ovens. This product provides a solid and secure installation. The ABS … Continue reading →
Baseboarders baseboard heater covers offer several important benefits for home renovation projects (or even new construction): Their unique perforated design can enhance the look of any room The covers may be spray-painted or cut to size for further customization Do-it-yourself … Continue reading →
At SupplyHouse.com, our goal is to bring you the highest quality plumbing, heating and HVAC supplies at competitive prices. Our product catalog includes PEX Plumbing Supplies, Radiant Heat Supplies, VisionPro Honeywell Thermostats, Taco pumps and mini-split air conditioners. If there are items you are looking for but can't find on our website, please contact our Customer Service Representatives & we will do our best to find what you need.
© 2015 SupplyHouse.com
Connect With Us: