Boiler Room |
Radiators & TrimGas Products |
Specialties |
Your new password is on its way. If you have problems accessing your account, please contact us at 1-888-757-4774 and we'll help you out.
I'm sorry, your e-mail was not found in our system.
If you think this is a mistake, please contact customer service at 1-888-757-4774 or via e-mail here.
You will have the option to create an account on the order confirmation page.
PEX tubing normally falls into two main categories: PEX with an oxygen barrier and PEX without an oxygen barrier. PEX with an oxygen barrier is designed for closed-loop space heating systems, and will normally be either red or white. It … Continue reading →
Fasco Motors have arrived at SupplyHouse.com just in time for the heating season! Fasco Motors manufactures top of the line OEM replacement Motors and Draft inducers for the biggest names in the HVAC industry. Here you can find replacements motors … Continue reading →
Looking for a comfortable even heat throughout your home that is both cost-effective and energy efficient? Consider the benefits of a radiant floor heating system to do the job. Drafts got you down? If your goal is to achieve even, … Continue reading →
When you’re picking a new bathroom ventilation fan, you will often come across the term ‘CFM.’ An abbreviation for cubic feet per minute, CFM quantifies the amount of air that a fan can move. Larger bathrooms require fans with higher … Continue reading →
SharkBite push-fit fittings revolutionized plumbing and hydronic heating, making installations and repairs faster and easier for professionals and do-it-yourselfers alike. Previously available in sizes only up to 1”, SharkBite now makes fittings for larger pipe. SharkBite 2XL fittings work with … Continue reading →
Unlike many local supply houses, SupplyHouse.com stocks and has access to thousands of replacement HVAC parts from the most popular brands in the industry such as Carrier, Trane, Barber Coleman, Lennox and Furnas Controls among many others. We recently added … Continue reading →
Ever wonder why so many of the old radiators you see are painted silver? Back in the day, they were mostly plain grey metal, but then the Spanish Influenza arrived during the winter of 1918-19 and that changed everything. So … Continue reading →
At SupplyHouse.com, our goal is to bring you the highest quality plumbing, heating and HVAC supplies at competitive prices. Our product catalog includes PEX Plumbing Supplies, Radiant Heat Supplies, VisionPro Honeywell Thermostats, Taco pumps and mini-split air conditioners. If there are items you are looking for but can't find on our website, please contact our Customer Service Representatives & we will do our best to find what you need.
© 2015 SupplyHouse.com
Connect With Us: